HIWIN Technologies Corp. is one of the world`s largest supplier of linear motion equipment. The company is capable of rolling out a full range of product lines in the linear-motion field with major products comprising precision ballscrews, linear guideways, and single axis robot.
Since its inception, HIWIN has been voted to deliver value-added products and solutions to customers from around the world. The company acquired the ISO9001, ISO14001 and OHSAS certificates in 1992, 1997 and 2002, individually.
To allow the best conditions for precision mechanical parts production, HIWIN plants the world over were designed to ensure an environment with constant temperature, stable humidity, and zero vibration.
HIWIN`s Spuer S ballscrew is developed to cope with the needs for advanced linear motion products. The Super S features high acceleration and high stiffness, low noise, high precision, high reliability, environmental friendly and energy saving. This patented design can deliver less impact, increase smoothness and better friction stability during circulation.
The Super S also features the special single pathway design which can reduce ball nut diameter by 32% smaller. The patented design of the return unit absorbs the noise of impact caused by the ballnut`s balls, greatly reducing the noise 5-7dB lower than traditional ballscrews. The Super S` up to 220,000 high Dm-N has became the highest Dm-N ballscrew in the world and is perfect for all kinds of CNC (computerized numerically controlled) machinery, automation equipment, semi-conductor and optoelectronics industries.
The company`s high rigidity roller type linear guideway RG series features a roller design instead of recalculating steel balls and offer super high rigidity and very high load capability. The RG series is ideal for automation systems, transportation equipment, CNC machining centers, heavy-duty cutting machines, CNC grinding machines, injection molding machines, plano millers, electric discharge machines and devices that require high rigidity or high load capacity.
With a strong management team and powerful global resource integration capability, HIWIN continues to engage in the production of high-tech, precision, and high-value-added products. From single components, subsystem components, system components, to the complete machine development, HIWIN fully exploits advantages of industrial manufacturing capability, mechanical engineering know how, and world class manufacturing cost control system to establish a new standard of "total solution.
HIWIN Technologies Corp.
Tel: 886-4-2359-4510 Fax: 886-4-2359-4420
E-mail: businesss@mail.hiwin.com.tw
Website: www.hiwin.com.tw (by Ben Shen)